This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC2642R: BLE pairing with passkey

Part Number: CC2642R

Tool/software: Code Composer Studio

Hi,

I'm Using CC2642r with Simple_peripheral project.

I'm trying to set GAPBondMgr in order to get passkey on BLE connection and encryption .

i'm using this code :

uint8_t pairMode = GAPBOND_PAIRING_MODE_INITIATE;
uint8_t mitm = TRUE;
uint8_t ioCap = GAPBOND_IO_CAP_DISPLAY_ONLY;
uint8_t bonding = TRUE;

GAPBondMgr_SetParameter(GAPBOND_PAIRING_MODE, sizeof(uint8_t), &pairMode);
GAPBondMgr_SetParameter(GAPBOND_MITM_PROTECTION, sizeof(uint8_t), &mitm);
GAPBondMgr_SetParameter(GAPBOND_IO_CAPABILITIES, sizeof(uint8_t), &ioCap);
GAPBondMgr_SetParameter(GAPBOND_BONDING_ENABLED, sizeof(uint8_t), &bonding);

instead of getting passkey to set i got "Authentication failed" .

if there something i need to in project environment in order to be able to use these BLE features ( defines , includes ... )?

Thanks