Part Number: CC2541
Other Parts Discussed in Thread: CC2592
We made several boards with the CC2541 and CC2592 front end. All got FCC approval and the CE mark back in 2016.
Now we are getting them re-certified and are seeing half harmonics to boards that did not change.
Most of the filtering is done in the CC2541 and CC2592s. There are PI filters and other passives.
Where are places to look for a solution? What causes half harmonics when you use the Continuous Wave tone and the Modulated counterpart?
2.402GHz unmodulated has the smallest half harmonic. 2.44GHz unmodulated and 2.48GHz unmodulated have half harmonics almost as large as the main signal. Modulated is worse for all.
Thanks, Tim.