Hi,
I gathered from SIG's website BLE technical factsheet that BLE is able to support unlimited nodes via a Star-Bus Network Topology. Few questions:
1) What is the max active/silent nodes per 'Star' cluster and the max no of nodes that can communicate on the Star-bus at any one time. Any documentations available for the BLE star-bus network topology that I can reference?
2) Which of the chipset(s) supports this topology... CC2540, CC2564 or CC2560. Please advise if it is one or more of the listed chipsets or if there are any other components which I may have missed out?
3) Given that this network topology is a published capability for BLE, are there TI template solutions (source codes, etc) for the implemention of a Star-Bus Network Topology via the chips in Question 2).
4) If there are no template solutions in question 3), how can I go about implementing this network topology via the chips in question 2)?
Please advise.
Thanks and Regards,
Selly