This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LAUNCHXL-CC26X2R1: Sending/Receiving binary data via XDS100UART

Part Number: LAUNCHXL-CC26X2R1


Tool/software: Code Composer Studio

Dear team,

Currently the LAUNCHXL-CC26X2R1 uses the Display driver in simple_peripheral.c to get data from the device to the PC. I was curious if there is a more light weight way e.g. work directly over UART. Given is link to something similar to what I would like to do, but I am not sure of the connections are there to use this driver code.

Link:

http://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/tirtos/2_14_03_28/exports/tirtos_full_2_14_03_28/docs/doxygen/html/_u_a_r_t_c_c26_x_x_8h.html

Best regards,

Connor Desmond