This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2564C: Total I/O Current consumption in Active Mode

Part Number: CC2564C

Hi There, in the CC2564C datasheet, the only reference I can find to the current consumption of the 1.8V digital IO rail is the following:

"Total I/O current consumption in active mode: 1mA (max)"

How is this defined? Does this 1mA mean the current consumption when the GPIO block is active but no load connected?

I guess the stuff that gets connected to the GPIO is then added to that 1mA?  Correct?

Please comment

Thanks!