This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650: LED light is not lit when connected to debug probe

Part Number: CC2650
Other Parts Discussed in Thread: UNIFLASH, ,

I have a Sensortag CC2650. I connected it to a debugger board, and the debugger board is in turn connected to a USB-type B cable to my laptop, where I have installed UniFlash.

However, I do not seem to be able to connect to the sensortag. The LED light on the sensortag is not lit after the connection, and I get an icepick error when I try to flash a program onto the sensortag. I know the USB cable is fine since upon the initial connection, the sensortag does flash a red light briefly, and whenever I press the reset button the LED light will also flash red briefly. Based on my understanding, the LED light on the sensortag should be green when it is connected, but in this case it is not lit at all after I connect it. What could be wrong here? Is my sensortag spoilt?

P/S I tried with another USB cable as well. The issue persisted.

Here is a short video showing what happens when I reset the sensortag (twice):