This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC26X2R1: Transfer 4kB File

Part Number: LAUNCHXL-CC26X2R1


Hi,

I'm having some difficulties to decided how I should solve the following problem. I would need to have two identical CC26x2 both send a 4kB large file (e.g. jpeg image) to each other, once they are connected.

During the connection of these two devices, they are each both a GATT Client & Server (due to multi_role).

What would the best way to transfer a 4kB large File (e.g. JPEG Image) from one CC26x2 to another CC26x2 (and vice versa).

Is it quicker to do it via GATT_Write, GATT_WriteLong or maybe even over GATT_Read?

How long should this whole process take about when using the PHY @ 1Mbps?

I'm currently using the SimpleLink CC13x2 26x2 3.20.0.68 BLE5 SDK (with multi_role project)

Thanks in advance!

SPEEDBIRD