Hello!
I can't seem to be able to find RTLS agent folder from the newest SDK for CC2640R2 launchboard. Is it not included anymore?
Another question which is kind of related. I am currently trying to evaluate AoA with 3x CC2640R2 boards and one BOOSTXL-AOA.
There are couple of issues: I can get it to work only with one configuration, which is the one where passive device does the AoA measurement and masters device is only holding the connection. But this only works if I have master device as RX in AoA capabilities. According to the simple link example this is not supposed to be the case. If i turn off the RX capabilities of the master, I cannot enable AoA from the RTLS UI anymore.
Also I am able to enable the AoA at RTLS UI when using only master device without passive, but in that case no AoA data is received at all.
Hope my explanations made any sense.