Part Number: CC2642R
Other Parts Discussed in Thread: BLE-STACK
Tool/software: Code Composer Studio
Hi
I am developing blue-tooth application on CC2642. Working with an example project named "project_zero" in BLE5 folder of the examples.
While trying to down the run "project zero" in my launch pad I got following problem. Please refer to the console window output shown below. I see that the last line of the below error message keeps repeating non-stop.
I thought of bringing the launchpad back to factory default condition by following the below link suggested by TI(shown below), but the problem persists. Please suggest me about how to recover from this issue. Thanks in advance.
Link to bring back factory image: http://software-dl.ti.com/simplelink/esd/simplelink_cc26x2_sdk/2.10.00.44/exports/docs/thread/html/ble-stack-oad/revert-to-factory.html
Environment details:
SDK version is simplelink_cc13x2_26x2_sdk_4_10_00_78
Development Studio: CCS10.0
Host is: Windows10 laptop.
Host interface: USB port of Launchpad CC2642
TARGET HW: LAUNCHXL - CC26X2 REV B, SDK 2.40
;*************************************************************
Cortex_M4_0: GEL Output: Memory Map Initialization Complete.
Cortex_M4_0: GEL Output: Board Reset Complete.
Cortex_M4_0: Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.1.0.00001)
Cortex_M4_0: Trouble Halting Target CPU: (Error -2064 @ 0x0) Unable to read device status. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.1.0.00001)
Cortex_M4_0: Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.1.0.00001)
;**************************************************************
Regards,
Pothirajan.K