This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/SIMPLELINK-CC2640R2-SDK: AoA using linux

Part Number: SIMPLELINK-CC2640R2-SDK


Tool/software: Code Composer Studio

Dear experts,

I am getting the following error when trying the example with multi-connection of the AoA application on a raspberry pi with a Rasbian Os.

=== ERROR: No one of the nodes identified as RTLS MASTER ===

I am able to identify the hardware serial port name: /dev/ttyACM1 and /dev/ttyACM0

And I am defining the devices list as follows:

devices = [ {"com_port" : "/dev/ttyACM1" , "baud_rate" : "460800", "name" : "CC26x2 Master"} ]

(I tried the different combinations os com port names: with and without dev, with and without slashes, and ACM0 and ACM1)

Any help is much appreciated.