This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LPSTK-CC1352R: I2C problem running BLE multi-sensor example

Part Number: LPSTK-CC1352R


Hi,

I have tried building and flashing the ble5stack multi-sensor example into the  LPSTK-CC1352R device (using CCS 10) but runs into problems with sensors.

Seem to be a problem to init the I2C-sensors (see below), the board works great with the default application that resides on the external flash.

Tried to read info about the example but is there any changes in configuration when running the example on LPSTK instead of LaunchPad (for which I guess its originally designed)?

I'm testing on SDK simplelink_cc13x2_26x2_sdk_4_10_00_78.

Best regards, TMA

#000001 [ 0.023 ] INFO: (multi_sensor.c:333) ==============================================================

#000002 [ 0.026 ] INFO: (multi_sensor.c:373) OAD Opened successfully

#000003 [ 0.026 ] INFO: (multi_sensor.c:381) OAD Image version: 0001

#000004 [ 0.027 ] INFO: (sensor_common.c:304) Sensor task started

#000005 [ 0.027 ] INFO: (sensor_common.c:337) I2C handle opened

#000006 [ 0.027 ] ERROR: (temp_profile.c:189) HDC sensor failed to open

#000007 [ 0.027 ] ERROR: (temp_profile.c:165) Temperature Profile failed to initialize with status 0x1

#000008 [ 0.027 ] ERROR: (hum_profile.c:185) HDC sensor failed to open

#000009 [ 0.028 ] INFO: (hum_service.c:260) Humidity Service initialized

#000010 [ 0.028 ] INFO: (hum_profile.c:157) Humidity Profile Initialized

#000011 [ 0.028 ] ERROR: (light_profile.c:180) OPT sensor failed to open

#000012 [ 0.028 ] ERROR: (light_profile.c:156) Light Profile failed to initialize with status 0x1

#000013 [ 0.028 ] INFO: (led_profile.c:112) LED's opened

#000014 [ 0.029 ] INFO: (led_service.c:250) LED Service initialized

#000015 [ 0.029 ] INFO: (led_profile.c:133) LED Profile Initialized

#000016 [ 0.029 ] INFO: (button_profile.c:101) Buttons enabled

#000017 [ 0.029 ] INFO: (button_service.c:245) Button Service initialized

#000018 [ 0.029 ] INFO: (button_profile.c:115) Button Profile Initialized

#000019 [ 0.030 ] INFO: (batt_service.c:198) Battery Service Initialized

#000020 [ 0.030 ] INFO: (batt_profile.c:130) Battery Profile Initialized

#000021 [ 0.030 ] INFO: (accel_service.c:402) Accelerometer Service initialized

#000022 [ 0.034 ] INFO: (multi_sensor.c:875) Tx Power successfully updated

#000023 [ 0.034 ] INFO: (multi_sensor.c:722) Device has started with address: 80:6F:B0:F0:25:E2

#000024 [ 0.034 ] INFO: (multi_sensor.c:728) Name in advertData array: Gluetec-Sensor

#000025 [ 0.038 ] INFO: (multi_sensor.c:954) Adv Set 0 Enabled

#000026 [ 0.048 ] INFO: (multi_sensor.c:954) Adv Set 1 Enabled