The application scenarios:
1.One battery powered collector node, 3 ~ 4 different kinds of battery powered meters (flow/temperature/pressure) as field nodes, transmitter nodes will send data to collector at intervals of 15 seconds to 30 seconds;
2.100 to 200 bytes per communication message
3. Support broadcast or other communication mode to save the power
4. Power consumption requirement of the collector and meters need within 50uA.
5. Field meters may have 1~2mm water film once water has accumulated (meter is metal housed), communication distance to collector is 1~2 metres. Transmission power may be increased when taking water film into account.
Question:
1. Could CC2642R meet the requirements above especially the <50uA even for the collector node?
2. Does there any reference design is similar to this application? Could you please share the resources(app note/sdk)?
Thank you so much
Best Regards,
Tess Chen