This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650MODA: Maximum Number of Simultaneously Transmitting CC2650MODA's

Part Number: CC2650MODA
Other Parts Discussed in Thread: CC2650

Hi,

I saw on the "CC2650MODA: CC2650 maximum throughput" thread on this forum that the CC2650 LaunchPad example can sustain a 300kbps link. Is it possible for multiple CC2650MODA modules to transmit at this datarate simultaneously to a single endpoint? If so, is there a limit to how many CC2650MODA modules could transmit simultaneously at this datarate to a single end point?

Thanks, ER