Hi,
I am designing my own PCB board using the CC2652R1. I have a few questions regarding the connection of some pins.
1. How do I connect the nReset pin? Do I need to connect it?
2. What pins do I use to load my programm onto my microcontroller? (cJTAG?)
3. Is it necessary to connect an external oscillator or can I just use the internal oszillator?
4. I could not import the Inverted_Antenna.dxf file into eagle, so I had to draw it myseld, but there were some distances and an angle missing. I am not suer if I missed somthing.