Part Number: CC2541
Tool/software: WEBENCH® Design Tools
Hi
I am trying to program the CC2541 with a simple SW code that wrote, but it doesn't work!
I am using AIR Embedded Workbench IDE and Texas Instrument 's CC Debugger that connected to a board with CC2541 chip.
After I push Make bottom, I push Download and Debug bottom, and I get the following messages in the log:
Sun May 24, 2020 20:33:13: IAR Embedded Workbench 10.30.1 (C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.1\8051\bin\8051proc.dll)
Sun May 24, 2020 20:33:14: Using license: Evaluation license - IAR Embedded Workbench for 8051, Evaluation edition 10.30
Sun May 24, 2020 20:33:14: Download complete.
Sun May 24, 2020 20:33:14: Loaded debugee: C:\Texas Instruments\BLE-CC254x-1.5.1.1\Projects\ble\SimpleBLEObserver\CC2541DB\CC2541EM\Exe\SimpleBLEObserver.d51
Sun May 24, 2020 20:33:14: Target reset
The problems is:
1. I get the same message even when the CC Debugger is disconnected.
2. The Chips isn't working ( it should turn on a led on the board using CC2541 GPIO/
I have also noticed that if I go to Project -> Download-> all the three options are turned off ( Download Active Application etc).
thanks
Gil