This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LPSTK-CC1352R: Multisensor problem

Part Number: LPSTK-CC1352R


Tool/software: Code Composer Studio

Hi everyone,

I am working currently on the sensortag LPSTK CC1352-R1F3. I tried to debug the multisensor project on the sensortag but it doesn't work. The hardware for the jtag connection and the RX/TX connections are good and i have this from my terminal. But i can't see on simplelink starter or BLE scanner the sensortag just as if the sensor doesn't advertise which is strange because the project multisensor was running. If someone could help me on my problem that would be nice.

Sincerely,

PERRIN Paul-Emile