This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC2564C: How long is the Bluetooth transmission delay normal?

Part Number: CC2564C

Tool/software: Code Composer Studio

 Hi,dear Ti engineer!

The two SPP devices A and B have established a connection. The point of HCI UART TX of the A device has finished sending a frame of HCI package is Time1,  The point of HCI UART TX of the B device start to transmit bt's receive data is Time2,The difference between Time2 and Time1 is a few milliseconds or tens of milliseconds. is this normal?

I want to achieve data transmission at close range and low latency (a few milliseconds),But the status quo is not ideal now.Thanks!

Best regards

Li