Part Number: CC256XSTBTBLESW
Other Parts Discussed in Thread: CC2564MODNEM,
Hello,
I am working with the following system: STM3240G-EVAL Board + CC256XEM-STADAPT Board + CC2564MODNEM Board and I am exploring the CC256XSTBTBLESW.
I have not an external codec mounted on the CC256XEM-STADAPT Board, but I am successfully running the AUDDemo using the STM3240G-EVAL Board DAC.
Now I would like to configure my board as an headset, to send and receive audio data, so I am running the HSPDemo.
After the OpenServer command, I can successfully connect to my smartphone and, when I start a call, I see the Audio Connection indication, but I cannot see any etHDSET_Audio_Data_Indication event coming.
Am I missing something? Does this demo need an external codec mounted on the CC256XEM-STADAPT Board?
Is it correct to expect that should be possible to receive audio data from the smartphone and send them back to the DAC through the I2S, adding the missing implementation?
Thank you for your help
Arianna