Other Parts Discussed in Thread: SYSCONFIG
Tool/software: Code Composer Studio
Hi all,
can somebody please help me.
I managed to run the project Zero.
now I want to transfer the code to a custom PCB, for starters I have to change the LED Pins and there the trouble starts....
I used the syscfg utility to change the PIN from IO_6 to IO_0 , leaving the name as is!
compiling......
Error: CONFIG_PIN_RLED not defined
I change the Pin back to IO_6
compiling......
Error: CONFIG_PIN_RLED not defined
Ti_drivers_config.h
has got the defines for the LEDs
#define CONFIG_PIN_GLED 0x00000007
#define CONFIG_PIN_4 0x00000006
but the sysconfig utility shows the name as
CONFIG_GPIO_RLED
CONFIG_GPIO_GLED
it says the file Ti_drivers_config.h is created by the SW, but where the ... does it get the #define CONFIG_GPIO_GLED from???
best regards
Kurt