This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652RB: txPower IB bits 0-6 and GC bits 6-7.

Part Number: CC2652RB

Hi Champs,

According to txPower register in "Table 25-48. CMD_SET_TX_POWER Command Format" in the TRM .
It says that IB:  Bit 0 to 6  and GC : Bit 6 to 7.
I seems Bit 6 is overlapped. 
Is it correct?

How can I understand the overlapped bit 6?
Thank you for your kind clarification.
Best regards,
Hitoshi