This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC2652R: Enable notifications

Part Number: CC2652R

Tool/software: Code Composer Studio

Hello,

a problem has occurred when using notification. When I connect to the Launch Pad with my mobile phone and enable the notifications for one characteristic, it is not possible to switch on the notification for the same characteristic with a second connection, e.g. a mobile phone. The characteristic always returns to OFF, again the first connection stays ON.
Only when I have disconnected from the Launch Pad and reconnected with both phones I can enable the notifications for both.

I use the SDK: "simplelink_cc13x2_26x2_sdk_3_20_00_68" and the Launch Pad CC26x2R with the multirole project.