Part Number: CC2640R2F
Hi,
A customer is testing AOA example,his enviroment is: LAUNCHXL-CC2640R2+BOOSTXL-AOA ,SDK: simplelink_cc2640r2_sdk_3_40_00_10
During the test, the time of HOST received RTLS_CMD_CONN_PARAMS was T1, then it was forwarded to passive device, and the time of passive received it was T2. They found that if the time difference between T1&T2 was larger than 250ms, the passive device could not receive the AOA data in subsequent procedure. This test is under 4G network, so is this because of network delay?
Can you please shed some light on solving this problem? thanks.
BR,
Viki