This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2564C: DO NOT want to use the LDOs in cc2564c

Part Number: CC2564C


Hi Team,

My Customer have further questions about the Power pin connections., in particular to the following pins
MLDO_IN, MLDO_OUT
CL1.5_LDO_IN, CL1.5_LDO_OUT
They have a 1.8V source in their circuit and DO NOT want to use the LDOs in cc2564c.
We plan to connect :
VDD_IO and VDD_IN to 1.8 V
Could you advise on connections to MLDO_IN, MLDO_OUT, CL1.5_LDO_IN, CL1.5_LDO_OUT?

Thank you
Renan