Part Number: CC2652RB
Other Parts Discussed in Thread: CC2652R
Hi Experts,
A customer would like to adjust the XOSC_HF frequency for each their board by change the value of Cap-Array Delta.
It seems that Cap-Array Delta can be modified following the thread below.
However, it requires to modify the CCFG.c.
Am I correct?
The customer would like to modify the Cap-Array Delta at the production line some how.
For example, CC2652RB is running like a maintenance mode and communicating with PC by SPI, UART, BLE, etc.
The command is prepared to change the Cap-Array Delta.
The procedure is as follows:
1. Continuous Tx at specified ch.
2. Freq. is measured.
3. Cap-Array Delta is modified.
4. Repeat from 1 to 3 and then the data is saved onto Flash.
5. Read the value by a prepared command.
6. Start running with the value at 4.
Could you please let us know whether it can be modified during it is running or not?
Also, could you please let us know if the value of Cap-Array Delta on flash can not be written with JTAG connection?
Thank you so much in advance for your advice.
Best regards,
Hitoshi