Part Number: CC2642R
Hi
I'm developing a central that should be able to connect up to 4 peripherals, with the lowest possible connection interval.
When connected to the first peripheral, if the connection interval is set to 7.5ms, the central is no longer able to scan for the next peripheral.
I tried to setup different scan window / scan interval but no way to make it scanning again.
Increasing the connection interval to 12.5ms (max connection interval = 12,5ms, min connection interval = 7.5ms) allows to scan and connect to the next peripheral, but I need to reduce that connection interval.
Is there a solution to handle this issue ?
Should I increase connection interval to allow more peripherals to be scanned ? then, once all connections are established, is it possible to decrease connection interval.
Another question is what is the min connection interval when multiple peripherals are connected to a single central ?
Is is 7.5ms x Nb of connected peripherals ?
Thanks for your help
Jerome