Part Number: CC2541
Hi! I'm trying to use timer 4 to generate an 1MHz interrupt to count microsseconds precisely, however it's not working well. Here's my code:
//Timer 4 Setup function
void Timer4_init(void)
{
//******************** Timer4, channel
// Timer 4 channel 0 compare value.
CLKCONCMD = (CLKCONCMD & ~CLKCON_TICKSPD) | CLKCON_TICKSPD_32M;
T4IE = 1;
/***************************************************************************
* Timer 4 setup
*
* Timer 4 channel 0 compare value. Initiates the Timer terminal count value
* to 224. This value is reseted at each Timer compare match interrupt.
*/
T4CC0 = e0;//224 -> 256 - (32MHz/(Prescaler*Target_Frequency)): Target_frequency=1MHz
/* Timer 4 channel 0 (T4CCTL0) configuration:
* - Channel 0 interrupt enabled.
* - Compare mode.
*/
T4CCTL0 = T4CCTLn_IM | T4CCTLn_MODE;
/* Timer 4 control (T4CTL) configuration:
* - Prescaler divider value: 1.
* - Modulo mode.
* The Timer is also cleared and started.
*/
T4CTL = T4CTL_DIV_1 | T4CTL_MODE_MODULO | T4CTL_CLR | T4CTL_START;
}
//Interrupt function
#pragma vector = T4_VECTOR
__interrupt void t4_isr(void)
{
// // Clears the module interrupt flag.
T4OVFIF = 0;
static uint16 micros = 0;
micros ++;
// Clears the CPU interrupt flag.
T4IF = 0;
}