This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc2540 stack: can a master update connection parameters?



Hi,

I understand that a peripheral device (slave) could send "connection parameter update request" to the master. Can a master actively initiate such an update?

Thanks a lot.

-Felix

  • Yes, the slave must directly call the HCI to do that. For a single-chip application, use the HCI API function HCI_LE_Connection_Update. If you are using a network processor configuration (such as with the USB Dongle), you can send the HCI "LE Connection Update Command". This command is defined in Volume 2, Part E, section 7.8.18 (page 1081) of the BT 4.0 spec.

  • Willis, Thank you for the rapid reply.

    Just to make sure - do you mean *slave* or *master* in your post? Since I'm concerned with the master.

    Thanks a lot!

    -Felix