Part Number: CC2640R2L
Other Parts Discussed in Thread: CC2640R2F, LAUNCHXL-CC2640R2
Hi Team,
Quick question as I am not familiar with the CC26xx SDK information. Will a design on the CC2640R2F be easily portable to the CC2640R2L. The SDKs are the same, but want to verify what needs to be considered.
How can we test that we can build firmware that supports the CC2640R2L without creating custom hardware for it first? Since it is the same SDK and the suggested development platform (LAUNCHXL-CC2640R2) uses the CC2640R2F it looks like it should run and build successfully even if the firmware requires something that the CC2640R2L does not support.
Basically, I want to asses if our existing firmware can be run on the CC2640R2L?
Regards,
Ramon