Part Number: CC2642R-Q1
Other Parts Discussed in Thread: SYSCONFIG
Tool/software: Code Composer Studio
The default TX POWER of Simple Peripheral project is 0dBm . However , the TX POWER should be changed to 5dBm in order to improve BLE transmition distance .
In order to verify which configuration setting parameter can change the default TX POWER , the HOST TEST project and CC2652 Launchpad were used , as shown in picture 1 . The macro
definition DEFAULT_TX_POWER was set to HCI_EXT_TX_POWER_5_DBM , as shown in picture 2 . Testing the actual TX POWER of CC2652 through R&S CMW500, as shown in picture 3 . The testing result
is shown in picture 4 .
Neither the DEFAULT_TX_POWER was set to HCI_EXT_TX_POWER_5_DBM or HCI_EXT_TX_POWER_0_DBM , the actual TX POWER of CC2652 stayed the same . How to change the default TX POWER in CC2642 ?
Where is my configuration wrong ?
picture 1 CC2652 Launchpad
picture 2 My DEFAULT_TX_POWER configuration
picture 3 R&S CMW500
picture 4 TX POWER testing result
1.My develop environment:
(1)CCS: Code Composer Studio 10.0.0
(2)SDK: simplelink_cc13x2_26x2_sdk_4_10_00_78
(3)hardware:CC2652 launchpad develop kit
2.Attachments(1)ble5_host_test_cc26x2r1lp_app-0dbm-capArray0X00.hex : DEFAULT_TX_POWER was set to HCI_EXT_TX_POWER_0_DBM
(2)ble5_host_test_cc26x2r1lp_app-5dbm-capArray0X00.hex : DEFAULT_TX_POWER was set to HCI_EXT_TX_POWER_5_DBM
attachments can be downloaded here: