Part Number: CC2564C
Hi,
I was wondering about the firmware update procedure for the CC2564C and its possible compatibility with Bluetooth 5.2, especially LE Audio feature and EATT layer.
Is it possible to update the CC2564C firmware via UART with HCI commands and a binary file ? If it is, what would be the procedure ? And would it be possible in a near future to update the CC2564C with a TI firmware that would make the CC2564C compatible with the new Bluetooth standard 5.2, at least theoretically ? Or is the component already 5.2 ready as it is ?
Thanks in advance for your answers.
Pierre