This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hello, I am somewhat new to CCS so this may be a relatively simple question but I am having some issues getting a slightly modified version of the simple_peripheral file that I have edited to interact with sensor controller to build without any errors. Specifically, the program is not recognizing the simplePeripheral_enqueueMsg() function nor the user_enqueueRawAppMsg() function. This results in the following error:
Description Resource Path Location Type
#10010 errors encountered during linking; "simple_peripheral_CC26X2R1_LAUNCHXL_tirtos_ccs.out" not built simple_peripheral_CC26X2R1_LAUNCHXL_tirtos_ccs C/C++ Problem
<a href="file:/C:/ti/ccs1010/ccs/tools/compiler/dmed/HTML/10234.html">#10234-D</a> unresolved symbols remain simple_peripheral_CC26X2R1_LAUNCHXL_tirtos_ccs C/C++ Problem
gmake: *** [all] Error 2 simple_peripheral_CC26X2R1_LAUNCHXL_tirtos_ccs C/C++ Problem
gmake[1]: *** [simple_peripheral_CC26X2R1_LAUNCHXL_tirtos_ccs.out] Error 1 simple_peripheral_CC26X2R1_LAUNCHXL_tirtos_ccs C/C++ Problem
unresolved symbol simplePeripheral_enqueueMsg, first referenced in <whole-program> simple_peripheral_CC26X2R1_LAUNCHXL_tirtos_ccs C/C++ Problem
This seems like an issue with a missing library or function definition, is there a file missing from my simple_peripheral directory that is responsible for this or is it something else? I have made sure to #include "scif.h" for this file as well.
Hi Caleb,
I agree that running through this lab that YiKai has positioned is a good first step. Our recommendation is to start with Sensor Controller Studio, build an image and then import to CCS. Let us know if there are any further questions after running through the lab.