Part Number: CC2564MODN
HI,
I need to connect to GNSS profile using Bluetopia, (Bluetopia 1.2 R2)
The GNSS profile is based on SPP profile:
https://www.bluetooth.com/specifications/profiles-overview/
Basically the problem comes down to be able to use SPP API functions from bluetopiaCoreAPI but with different UUID for the SPP
Standard SPP UUID is 0x1101
For the GNSS it is 0x1136.
How can I use SPP api to connect to this 0x1136 UUID?
if it is not possible what other options do I have with Bluetopia in this case?
Regards
Rafal