This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LAUNCHXL-CC2650: I can't program the board with simple_broadcater sample code

Part Number: LAUNCHXL-CC2650
Other Parts Discussed in Thread: UNIFLASH

Tool/software: Code Composer Studio

Hello,

I would like to test the example software for bluetooth communication.

I installed ble_sdk_2_02_04_06 and now I am trying to program the launchpad but without success.

Error:

Cortex_M3_0: GEL Output: Memory Map Initialization Complete.
Cortex_M3_0: Failed Board Reset: (Error -151 @ 0x0) One of the FTDI driver functions used during the connect returned bad status or an error. The cause may be one or more of: no XDS100 is plugged in, invalid XDS100 serial number, blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable. Use the xds100serial command-line utility in the 'common/uscif' folder to verify the XDS100 can be located. (Emulation package 9.2.0.00002)
Cortex_M3_0: GEL: Error while executing StartUp( 10, 1, 0, 2013 ): Reset failed: retcode=-1
at GEL_AdvancedReset("Board Reset") [cc26x0.gel:29]
at StartUp(10, 1, 0, 2013)

I thought it was a problem with the XDS100 but with other projects it works.

Thanks in advance for your reply,

Fabio