Hi all,
This is my 3rd post and my previous 2 questions haven't received any answer. Maybe they're stupid questions, so if they are, please let me know.
Anyway, I have one more question if anyone is able to reply:
On the CC2540 MiniDK Dongle, I've been trying to measure the received signal strength and it seems that the reported RSSI saturates at -33dB even with the keyfob right next to the dongle and transmitting at full power (4dBm). I'm fairly certain the reported RSSI is correct (i.e. no offset) since my tests with changing the Rx sensitivity on the dongle is noticeable. With the regular sensitivity, the link is lost when the RSSI reaches around -85dBm and with high sensitivity, the link is lost at around -95dBm.
I'm guessing the saturation is due to the dongle and not the keyfob because the RSSI saturates with the keyfob set at 0dBm output power and switching to 4dBm has no effect on the receive RSSI value.
I checked the Application Note for selecting antennas and for the Meandered Antenna design, I didn't see anything that could account for such a large loss.
Is this -33dB loss normal for these boards? Is there a design that can improve the link budget?
Thanks,
Vic.