Part Number: CC2640R2F
Other Parts Discussed in Thread: OPT3002
Hello,
I have a USB to UART w/ battery charger powering my CC2640r2 and peripheral four OPT3002 devices. When I'm connected to the debugger (via LaunchPad), I can compile, download and run the application. I can send commands via the USB port and collect optical readings from the OPT3002 - no problem. When I disconnect the debugger and power the device from the USB (or battery) the I2C bus no longer responds. I've checked the obvious stuff - supply voltages, gnd, etc. Is there something that the debugger is doing with respect to the I2C bus, Rx/Tx lines, or something else that would not happen if it were not connected and running in debug mode?
Any thoughts would be appreciated.
Patrick