Tool/software: TI C/C++ Compiler
Dear teams,
Have a nice day!
My customer is using STM32F103+CC2564B for their scanner gun. They used SPPLEDEMO and placed HID into it. Currently, there has three different mode, but not enabled at the same time. The freeRTOS's tickless mode has been enabled. The power consumption for different mode are nearly same with 20mA current when used for broadcasting. When it has connected, it has 27mA current consumption. Customer has tried to used "sniff" mode, but it does not works. Now, they try to let the stm32 enter "stop" mode, but it takes some time and Bluetooth will be disconnected.
So, they have tried to reduce the power consumption to minimum from hardware side. Do we have any way to reduce the power consumption further from software part?
Thanks!
Dylan (FAE)