Part Number: CC2640R2F
I am currently debugging a system with one device running the 2640R2F part, and another device running the 2642R1F. I am switching the XDS110 probe between the two devices to debug, depending on which device I am making code changes to. When I launch the debugger after switching, I get a message saying the probe requires a firmware download. The 2642R1F project is based on Code Composer Studio version 10 and the 2640R2F is based on Code Composer Studio version 8.3. On 3 occasions, the firmware download fails and the XDS110 is rendered useless. I cannot connect to it, I have tried the xdsdfu utility and it cannot connect nor execute any commands. I am on my 4th probe. This is getting frustrating to use the tools necessary to develop and debug an application on the TI BLE parts. Any help or suggestions how to avoid this issue would be appreciated.