Hello all,
I'm working on custom made cc2640r2f devices with stack simplelink_cc2640r2_sdk_4_20_00_04, xdc tools xdctools_3_51_03_28_core and ccs 9.3.
The extflash I'm using is FM25Q04 4M-bit Serial Flash Memory from Shanghai Fudan Microelectronics group company limited.
We store the data in the extflash to retain after the device is reseted.
I'm powering the cc2640r2f devices with coin cell of 3V battery capacity but when the devices runs out of the battery all the data stored in extflash gets erased.
Can anybody suggest us methods for saving the external flash data after battery is drained out.
Thanks in advance.
Please suggest.