Part Number: LAUNCHXL-CC26X2R1
I am trying to use the host_test example project to use the cc26x2 as a central and periferal device simultaneously. I can't find a way of doing this easely.
Where do start with this? I am using the SDK 4.20.00.35.
I saw that the configuration is custom. The RF Mode is declared as object "RF_modeBle", but I can't find this file, where I would suspect the role is configured.
We are using the host_test example because this has native NPI support as opposed to the multi_role example.
If there is a better way of implementing the multiple BLE role switching, I am open for suggestions. The end goal is to use multiple BLE roles (central and perifieral) in combination with RTLS master.
Thanks beforehand,
Ruben M.