Other Parts Discussed in Thread: SYSCONFIG
Dear All
I'm using a multirole app with latest CCS, SDK based on CC2642R.
When the app runs as a peripheral role, using Public address mode works fine when connected MacOS central.
When connecting to win 10, only one peripheral works fine, the first connected peripheral is paired / bonded successfully, other identical devices are not able to pair (pair fails with reason 8).
I switched to RPA with public ID address mode, and now win 10 is able to connect to multiple peripherals, this address mode solves the issue on Win 10, anyway, when connecting to MacOS, it still works but when the peripheral is disconnected, the Mac lists multiple peripherals available while only one was connected.
I'm a bit stuck on that current behavior, any help would be greatly appreciated.
Thanks