Part Number: CC2640R2L
CC2640R2L has only 1 uart, My customer need 2 uarts.
1.Can GPIO be used to simulate uart for communication?
2.If it is not feasible, is there any other way to solve it?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CC2640R2L
CC2640R2L has only 1 uart, My customer need 2 uarts.
1.Can GPIO be used to simulate uart for communication?
2.If it is not feasible, is there any other way to solve it?
Hi M-W,
Thanks for your reply. My customer would use 2 uarts at the same time, and there is not a Sensor Controller in CC2640R2L.
Hi Qixiang,
My bad, I read the part number/name a bit to fast. In the case of the "L" device, implementing a SW based solution is the only and best approach really. It could be that they could take advantage of the SPI module while doing so in order to lower the SW a bit but that would really only work for a TX only UART: