This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2642R: CC2642R Development Kit transmit power 5DB transmission distance is very short.

Part Number: CC2642R
Other Parts Discussed in Thread: RF-RANGE-ESTIMATOR

Hi all,

i test CC2642R Development Kit transmission distance.

result:

DevKit 0db DevKit 5db
iphone8 13.2.2 160m 175m
Samsung C7000 7.0 170m 190m

test step:

1.Fixed development board, 2m above the ground

2.It can be successfully connected far away from the development board, which is considered as an effective distance

My test results show that 0DB and 5db are only 20 meters apart.  I think this is abnormal.

sdk:  simplelink_cc13x2_26x2_sdk_4_10_00_78

demo:  simple_peripheral_oad_onchip

1.What is the normal distance according to my test?

2.How should I modify to get close to this result?