Part Number: CC2652R
Other Parts Discussed in Thread: UNIFLASH, SIMPLELINK-CC13X2-26X2-SDK,
Tool/software: Code Composer Studio
I know there are other ways to flash this board, I am specifically trying to make UART BOOTLOADER flash work to verify it will work in an actual design.
After flashing the HEX image of one of the standard projects, the application does not start.
I have a LAUNCHXL-CC26X1R1. It works fine when loaded via UniFlash or CCS using the USB debugger.
I am trying to program it via the integrated bootloader via the "Application/User UART" which is normally used to interface with the application.
My settings:
- Serial Connection > CC2652R1F(BOOTLOADER)
- Application Image 1: zed_light_CC26X2R1_LAUNCHXL_tirtos_ccs.hex
- COM3 (shows as "XDS 110 Class Application/User UART", and normally has the application interface. Putty is closed while using UniFlash)
Process:
- Hold BTN-1 / DIO13 while pressing RESET
- (Verify the application does not start)
- Press "Load Image" in UniFlash
Result:
- The flash process is reported to be successful (see below)
- After resetting the board, the application does not start (no application output on UART, no other behavior)
- The bootloader is also not starting (therefore I assume in the bootloader start flowchart "FLASH image valid?" must be true)
- Switching UniFlash to use the default XDS110 USB Debug probe and verifying the same hex file it immediately fails to verify at 0x00000040
- Programming the same hex file using the XDS110 USB Debug probe is successful.
[11/22/2020, 6:44:45 PM] [INFO] Cortex_M3_0: CC2652R1F(Bootloader) [11/22/2020, 6:44:45 PM] [INFO] Cortex_M3_0: Auto baud detection is successful! [11/22/2020, 6:44:45 PM] [INFO] Cortex_M3_0: Ping command is successfully received by target! [11/22/2020, 6:44:45 PM] [INFO] Cortex_M3_0: Erase sector on address :0x0 is succesful! [11/22/2020, 6:44:45 PM] [INFO] Cortex_M3_0: Erase sector on address :0x2000 is succesful! [11/22/2020, 6:44:45 PM] [INFO] Cortex_M3_0: Erase sector on address :0x4000 is succesful! [11/22/2020, 6:44:45 PM] [INFO] Cortex_M3_0: Erase sector on address :0x6000 is succesful! [11/22/2020, 6:44:45 PM] [INFO] Cortex_M3_0: Erase sector on address :0x8000 is succesful! [11/22/2020, 6:44:45 PM] [INFO] Cortex_M3_0: Erase sector on address :0xA000 is succesful! [11/22/2020, 6:44:45 PM] [INFO] Cortex_M3_0: Erase sector on address :0xC000 is succesful! [11/22/2020, 6:44:45 PM] [INFO] Cortex_M3_0: Erase sector on address :0xE000 is succesful! [11/22/2020, 6:44:45 PM] [INFO] Cortex_M3_0: Erase sector on address :0x10000 is succesful! [11/22/2020, 6:44:45 PM] [INFO] Cortex_M3_0: Erase sector on address :0x12000 is succesful! [11/22/2020, 6:44:45 PM] [INFO] Cortex_M3_0: Erase sector on address :0x14000 is succesful! [11/22/2020, 6:44:46 PM] [INFO] Cortex_M3_0: Erase sector on address :0x16000 is succesful! [11/22/2020, 6:44:46 PM] [INFO] Cortex_M3_0: Erase sector on address :0x18000 is succesful! [11/22/2020, 6:44:46 PM] [INFO] Cortex_M3_0: Erase sector on address :0x1A000 is succesful! [11/22/2020, 6:44:46 PM] [INFO] Cortex_M3_0: Erase sector on address :0x1C000 is succesful! [11/22/2020, 6:44:46 PM] [INFO] Cortex_M3_0: Erase sector on address :0x1E000 is succesful! [11/22/2020, 6:44:46 PM] [INFO] Cortex_M3_0: Erase sector on address :0x20000 is succesful! [11/22/2020, 6:44:46 PM] [INFO] Cortex_M3_0: Erase sector on address :0x22000 is succesful! [11/22/2020, 6:44:46 PM] [INFO] Cortex_M3_0: Erase sector on address :0x24000 is succesful! [11/22/2020, 6:44:46 PM] [INFO] Cortex_M3_0: Erase sector on address :0x26000 is succesful! [11/22/2020, 6:44:46 PM] [INFO] Cortex_M3_0: Erase sector on address :0x56000 is succesful! [11/22/2020, 6:44:46 PM] [INFO] Cortex_M3_0: Erasing memory time elapsed: 1.26s [11/22/2020, 6:45:35 PM] [INFO] Cortex_M3_0: Programming memory time elapsed: 49.03s [11/22/2020, 6:45:35 PM] [INFO] Cortex_M3_0: Number of bytes programmed: 169728 bytes [11/22/2020, 6:45:35 PM] [INFO] Cortex_M3_0: Programming speed: 3.38kByte/s [11/22/2020, 6:45:35 PM] [INFO] Cortex_M3_0: Verify memory at address :0x0 for 0x1FFC bytes, is match with the expected CRC : 0x3AC4EE02 [11/22/2020, 6:45:35 PM] [INFO] Cortex_M3_0: Verify memory at address :0x2000 for 0x2000 bytes, is match with the expected CRC : 0x5679483 [11/22/2020, 6:45:35 PM] [INFO] Cortex_M3_0: Verify memory at address :0x4000 for 0x2000 bytes, is match with the expected CRC : 0x7DAF4391 [11/22/2020, 6:45:35 PM] [INFO] Cortex_M3_0: Verify memory at address :0x6000 for 0x2000 bytes, is match with the expected CRC : 0xEFB6707B [11/22/2020, 6:45:35 PM] [INFO] Cortex_M3_0: Verify memory at address :0x8000 for 0x2000 bytes, is match with the expected CRC : 0x623A563C [11/22/2020, 6:45:35 PM] [INFO] Cortex_M3_0: Verify memory at address :0xA000 for 0x2000 bytes, is match with the expected CRC : 0x5593D0A9 [11/22/2020, 6:45:35 PM] [INFO] Cortex_M3_0: Verify memory at address :0xC000 for 0x2000 bytes, is match with the expected CRC : 0x1ECF194F [11/22/2020, 6:45:35 PM] [INFO] Cortex_M3_0: Verify memory at address :0xE000 for 0x2000 bytes, is match with the expected CRC : 0x57B796A4 [11/22/2020, 6:45:35 PM] [INFO] Cortex_M3_0: Verify memory at address :0x10000 for 0x2000 bytes, is match with the expected CRC : 0x1F9E3F81 [11/22/2020, 6:45:35 PM] [INFO] Cortex_M3_0: Verify memory at address :0x12000 for 0x2000 bytes, is match with the expected CRC : 0x5B9C29AB [11/22/2020, 6:45:35 PM] [INFO] Cortex_M3_0: Verify memory at address :0x14000 for 0x2000 bytes, is match with the expected CRC : 0xDDA719C7 [11/22/2020, 6:45:35 PM] [INFO] Cortex_M3_0: Verify memory at address :0x16000 for 0x2000 bytes, is match with the expected CRC : 0xD428ECCF [11/22/2020, 6:45:36 PM] [INFO] Cortex_M3_0: Verify memory at address :0x18000 for 0x2000 bytes, is match with the expected CRC : 0x21DF5E5B [11/22/2020, 6:45:36 PM] [INFO] Cortex_M3_0: Verify memory at address :0x1A000 for 0x2000 bytes, is match with the expected CRC : 0xCA6100E0 [11/22/2020, 6:45:36 PM] [INFO] Cortex_M3_0: Verify memory at address :0x1C000 for 0x2000 bytes, is match with the expected CRC : 0x7CD113A7 [11/22/2020, 6:45:36 PM] [INFO] Cortex_M3_0: Verify memory at address :0x1E000 for 0x2000 bytes, is match with the expected CRC : 0xCEAB69D9 [11/22/2020, 6:45:36 PM] [INFO] Cortex_M3_0: Verify memory at address :0x20000 for 0x2000 bytes, is match with the expected CRC : 0xEEFC5121 [11/22/2020, 6:45:36 PM] [INFO] Cortex_M3_0: Verify memory at address :0x22000 for 0x2000 bytes, is match with the expected CRC : 0x2E67AF3B [11/22/2020, 6:45:36 PM] [INFO] Cortex_M3_0: Verify memory at address :0x24000 for 0x2000 bytes, is match with the expected CRC : 0x9088E32D [11/22/2020, 6:45:36 PM] [INFO] Cortex_M3_0: Verify memory at address :0x26000 for 0x36AC bytes, is match with the expected CRC : 0xD3BC9DC5 [11/22/2020, 6:45:36 PM] [INFO] Cortex_M3_0: Verify memory at address :0x57FA8 for 0x30 bytes, is match with the expected CRC : 0x70A9D137 [11/22/2020, 6:45:36 PM] [INFO] Cortex_M3_0: Verifying memory time elapsed: 0.6301s [11/22/2020, 6:45:36 PM] [INFO] Cortex_M3_0: CCFG comes from the application image. [11/22/2020, 6:45:36 PM] [INFO] Cortex_M3_0: Reset is executed! [11/22/2020, 6:45:36 PM] [SUCCESS] Program Load completed successfully.