This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650: CC2650 PHY layer Packet structure

Part Number: CC2650


Dear Team

Good day!

Our customer need us to confirm that , whether the CC2650 can change the PHY layer Packet structure , because they want to  implement their own protocol for PHY.

Best regards,

 Leon.liu

  • Hi,

    Good day to you too!

    CC2650 can be used in BLE mode or in proprietary mode. In both cases, only operations in the 2.4GHz band are possible.

    You will find a few threads on the forum dealing with "CC2650 proprietary mode". In addition, you can use SmartRF Studio to see the possibilities offered by the CC2650 device.

    I hope this will help.

    Kind regards,

  • Hi Clément

    Thank you for your help .

    Does it mean that there are no other PHY layer packet structures other than "Simple packet format", and "Advanced packet format", packet format for BLE? I want to make sure there is no other option to build the original packet structure into CC2650.

    Kind regards,
    Leon.liu

  • Hi Leon,

    When using CC2650 you can also use your own proprietary packet format. To do so, please review the examples rfEasyLinkRx / rfEasyLinkTx and rfPacketRx / rfPacketTx within the SDK.

    I am not 100% sure to well answer your question. Please don't hesitate to provide some details on the use case you/they have.

    Kind regards,