If APCFG = 0xFF ( all Port 0 I/O are analog ones) and the op amp is turned on through OPAMPC |= 0x01 , does this operation prevent from considering also AIN0, AIN1, AIN2 as ADC inputs in the setup of a conversion sequence ? That is : if I program ADCCON2.SCH = 7 , the conversion sequence comprises also op amp pins or not (as would be logical) ?