Other Parts Discussed in Thread: CC2564C, CC2560
E2E Persons of Quality,
I am looking for a LaunchPad which can support the following:
1. Act as a source or sink for classic Bluetooth music streaming via A2DP.
2. Is supported by SmartRF Studio.
3. Can provide performance metrics as to RSSI, PER and effective throughput between (2) SmartRF nodes.
4. Has an App available for Android or IOS which could be configured as the source for testing against a SmartRF EVM node like the above.
5. Has an external antenna port.
6. Cost less than one dollar:-)
I am developing a system for use in a highly specialized, non-traditional environment.
Peace,
Jay Zebryk