Other Parts Discussed in Thread: LAUNCHXL-CC26X2R1
HI everybody ,
I need to perform the fw upgrade (starting from a .hex file) of the CC2642 installed on my board , where I don’t have the JTAG interface, but only serial pins availble
I m trying to use the follow setup but it is not working , why ? ( I m using a LP as bridge PC to my board )
- SmartRF Flash Programmer 2 ver. 1.8.2
- LAUNCHXL-CC26X2R1 (with all the jumpers that do the connection with the CC2652 removed)
- Connections between launchpad and CC2642 in meter module:
- GND and 3.3V
- UAR interface (RX and TX line)
- RESET
- SBWTCK line connected to 3.3V.
any other way I can make it ? anything I shoudl check ?
thank you
BR
Carlo