Hi,
I have a doubt regarding to the schematic of the keyfob (version 1.1.0 of the swrr071.zip document). There are two inductors (schematic reference L251 and L261) placed between the cc2540 and the antenna, which have a value of 2.0nH (L251=L_2N0_0402_S and L261=L_2N0_0402), but in the PARTLIST document they have assigned a diferent value: L_2N2:0402_S. What is the correct value? The one that appear in the SCHEMATIC or the one in the PARTLIST? It seems that it is more standard the value that appears in the PARTLIST, but which one is better to place in a new design?
Thanks!