Part Number: CC2652R
SDK: simplelink_cc13x2_26x2_sdk_4_30_00_54
Target: CC2652 LaunchPad
I'm trying to rebuild the StackWrapper project in CCS, but the result is unsuccessful with errors as below. It seems CCS can't find the build_config.opt while the file is actually under the StackWrapper folder.
I have tried copy the opt file into the TOOL foolder but with no luck. Please help give some tips for the proper project setup, thanks.
BTW, the project can build properly in IAR.
Description Resource Path Location Type #35 #error directive: "Build Configuration Error: At least one Controller build component required!" .ccsproject /Stack_Wrapper line 99, external location: C:\ti\simplelink_cc13x2_26x2_sdk_4_20_00_35\source\ti\ble5stack\inc\bcomdef.h C/C++ Problem Cannot open command file '/build_config.opt': No such file or directory ble_dispatch_JT.c /Stack_Wrapper/ICallBLE C/C++ Problem Cannot open command file '/build_config.opt': No such file or directory ble_dispatch_lite.c /Stack_Wrapper/ICallBLE C/C++ Problem Cannot open command file '/build_config.opt': No such file or directory common_rom_init.c /Stack_Wrapper/ROM C/C++ Problem Cannot open command file '/build_config.opt': No such file or directory gap.c /Stack_Wrapper/Host C/C++ Problem Cannot open command file '/build_config.opt': No such file or directory gapbondmgr.c /Stack_Wrapper/Host C/C++ Problem Cannot open command file '/build_config.opt': No such file or directory gatt_uuid.c /Stack_Wrapper/Host C/C++ Problem Cannot open command file '/build_config.opt': No such file or directory gattservapp_util.c /Stack_Wrapper/Host C/C++ Problem Cannot open command file '/build_config.opt': No such file or directory hal_assert.c /Stack_Wrapper/HAL/Common C/C++ Problem Cannot open command file '/build_config.opt': No such file or directory hal_flash_wrapper.c /Stack_Wrapper/HAL/Target/CC2650/Drivers C/C++ Problem Cannot open command file '/build_config.opt': No such file or directory icall_lite_translation.c /Stack_Wrapper/ICallBLE C/C++ Problem Cannot open command file '/build_config.opt': No such file or directory icall_startup.c /Stack_Wrapper/Startup C/C++ Problem Cannot open command file '/build_config.opt': No such file or directory npi.c /Stack_Wrapper/NPI C/C++ Problem Cannot open command file '/build_config.opt': No such file or directory onboard.c /Stack_Wrapper/TOOLS C/C++ Problem Cannot open command file '/build_config.opt': No such file or directory osal.c /Stack_Wrapper/OSAL C/C++ Problem Cannot open command file '/build_config.opt': No such file or directory osal_bufmgr.c /Stack_Wrapper/OSAL C/C++ Problem Cannot open command file '/build_config.opt': No such file or directory osal_cbtimer.c /Stack_Wrapper/OSAL C/C++ Problem Cannot open command file '/build_config.opt': No such file or directory osal_clock.c /Stack_Wrapper/OSAL C/C++ Problem Cannot open command file '/build_config.opt': No such file or directory osal_list.c /Stack_Wrapper/OSAL C/C++ Problem Cannot open command file '/build_config.opt': No such file or directory osal_memory_icall.c /Stack_Wrapper/OSAL C/C++ Problem Cannot open command file '/build_config.opt': No such file or directory osal_pwrmgr.c /Stack_Wrapper/OSAL C/C++ Problem Cannot open command file '/build_config.opt': No such file or directory osal_snv_wrapper.c /Stack_Wrapper/OSAL C/C++ Problem Cannot open command file '/build_config.opt': No such file or directory osal_timers.c /Stack_Wrapper/OSAL C/C++ Problem Cannot open command file '/build_config.opt': No such file or directory rtls_srv.c /Stack_Wrapper/Host C/C++ Problem Cannot open command file '/build_config.opt': No such file or directory sm_ecc.c /Stack_Wrapper/Host C/C++ Problem gmake: *** [Host/gap.obj] Error 1 Stack_Wrapper C/C++ Problem gmake: *** [Host/gatt_uuid.obj] Error 1 Stack_Wrapper C/C++ Problem gmake: *** [Host/gattservapp_util.obj] Error 1 Stack_Wrapper C/C++ Problem gmake: *** [Host/rtls_srv.obj] Error 1 Stack_Wrapper C/C++ Problem gmake: *** [Host/sm_ecc.obj] Error 1 Stack_Wrapper C/C++ Problem gmake: *** [ICallBLE/ble_dispatch_JT.obj] Error 1 Stack_Wrapper C/C++ Problem gmake: *** [ICallBLE/ble_dispatch_lite.obj] Error 1 Stack_Wrapper C/C++ Problem gmake: *** [NPI/npi.obj] Error 1 Stack_Wrapper C/C++ Problem gmake: *** [OSAL/osal_cbtimer.obj] Error 1 Stack_Wrapper C/C++ Problem gmake: *** [TOOLS/onboard.obj] Error 1 Stack_Wrapper C/C++ Problem gmake: Target 'all' not remade because of errors. Stack_Wrapper C/C++ Problem
BR,
Shuyang