This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LPSTK-CC1352R: Out-of-the-box only runs under debugger

Part Number: LPSTK-CC1352R

I used a 1352R launchpad to program my LPSTK with some 1352R sample programs - namely the optical sensor and temp/humidity.

So I tried the "hold button 1" down trick and that did not restore the ootb image. So I used the debugger to download the multi sensor image, and it would work fine under the debugger, but as soon as I tried it on battery power, I got no response. So, while running under the debugger I used the OAD download from my phone, and it seemed to download OK, but when I switched to battery power, no response.

Is there a trick to resetting the LPSTK? There is no reset button.